VM.PGMERRORLIST
Description
VM.PGMERRORLIST returns a list of items (such as recently added parameters) being used in the downloaded BASIC program which the installed firmware does not support. When the drive returns Fault 831 (BASIC program is invalid), you can either:
1. Use VM.PGMERRORLIST to identify and remove unsupported calls to items.
or
2. Upgrade your firmware, and then re-compile, and re-download the BASIC program.
General Information
|
Type |
R/O |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Start Version |
M_01-09-00-000 |
Variants Supported
This parameter is only supported on AKD BASIC drives.